SWRU473A February 2017 – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
Many sample applications come with UART support for printing the debug information, or status of any operation. Some applications require user input through the UART, so TI advises installing a serial terminal application. Tera Term is used for demonstration here, but the Code Composer Terminal may also be used. Follow these steps to instal Tera Term:
Be sure to install the XDS110 drivers for the PC to enumerate these ports for the serial terminal. Refer to Section 3.4 for installation of the XDS110 drivers.
Figure 2. Tera Term New Connection Window
Figure 3. Tera Term Serial Port Tab
Figure 4. Tera Term Serial Port Settings