SWCA305 May   2026 CC1350 , CC1352P , CC1352P7 , CC1352R , CC2340R2 , CC2340R5 , CC2340R5-Q1 , CC2540 , CC2541 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2640R2L , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2651P3 , CC2651R3 , CC2651R3SIPA , CC2652P , CC2652P7 , CC2652PSIP , CC2652R , CC2652R7 , CC2652RSIP , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10

 

  1.   1
  2. 1Summary
  3. 2Vulnerability
  4.   Trademarks

Summary

An issue identified in the Texas Instruments Bluetooth® stack causes a Denial of Service (DoS) condition. The potential vulnerability can be exploited by sending a crafted LL_Pause_Enc_Req packet during the Bluetooth LE connection establishment phase. When processed by an affected device, this malformed packet can cause the device to enter an unresponsive state, requiring a manual reset to restore normal operation.