SPRADE8 November 2023 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
In order to support EEPROM emulation with varying data sizes (other than 64-bits), the Flash Sectors selected for emulation are divided into a format referred to as EEPROM Banks (not to be confused with Flash Banks) and Pages. First, the Flash sector (or set of chosen Flash Sectors) is divided into EEPROM banks. Each EEPROM bank is further divided into Pages. This partitioning is shown in Bank Partitioning. The partitioning of EEPROM Banks and Pages is the same for Single-Unit and Ping-Pong emulation.
Using this format allows the application to:
Figure 3-3 Bank PartitioningThe first eight 16-bit words of each EEPROM bank are reserved for EEPROM bank status information and the first eight words of each page are reserved for page status information. Every time a new set of data is written to a page, the status location of the last page and the next page are modified. When a new EEPROM bank is used the Bank Status of the last and current EEPROM banks are updated. Both the EEPROM Bank and Page status words differentiate between the current EEPROM Bank/Page and a used EEPROM Bank/Page in the same way. To mark an EEPROM Bank or Page as current, the first 64-bits are written with the appropriate status code. To mark an EEPROM Bank or Page as full, the latter 64-bits are written with the appropriate status code. More details about the status codes can be found in the EEPROM_GetValidBank.
As seen in Page Layout, all pages contain an eight-word page status and a configurable amount of data space. Page 0 is slightly different as it contains the EEPROM bank status as well. Only Pages 0 and 1 are shown, but it should be noted that Page 2 through Page (N-1) are identical to Page 1.
Figure 3-4 Page Layout