SPRADE8 November 2023 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Choose which Flash Sectors to use for EEPROM emulation. The sectors chosen (if multiple) should be contiguous and in order from least to greatest. Insert only the First and Last sectors to be used for EEPROM. For example, to use sectors 1-10, insert {1,10}. To only use sector 1, insert {1,1}. A valid configuration will have the following properties.
More details about invalid or dangerous configurations can be found in Section 6.2.1.
uint16 FIRST_AND_LAST_SECTOR[2][2] = {1,1};