SPRADE8 November   2023 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   EEPROM Emulation for Generation 3 C2000 Real Time Controllers
  2.   Trademarks
  3. Introduction
  4. Difference Between EEPROM and On-Chip Flash
  5. Overview
    1. 3.1 Basic Concept
    2. 3.2 Single-Unit Method
    3. 3.3 Ping-Pong Method
    4. 3.4 Creating EEPROM Sections (Pages) and Page Identification
  6. Software Description
    1. 4.1 Software Functionality and Flow
  7. Ping-Pong Emulation
    1. 5.1 User-Configuration
      1. 5.1.1 EEPROM_Config.h
      2. 5.1.2 F28P65x_EEPROM.c
    2. 5.2 EEPROM Functions
      1. 5.2.1  EEPROM_Config_Check
      2. 5.2.2  Configure_Protection_Masks
      3. 5.2.3  EEPROM_Write
      4. 5.2.4  EEPROM_Read
      5. 5.2.5  EEPROM_Erase
        1. 5.2.5.1 Erase_Bank
      6. 5.2.6  EEPROM_GetValidBank
      7. 5.2.7  EEPROM_UpdateBankStatus
      8. 5.2.8  EEPROM_UpdatePageStatus
      9. 5.2.9  EEPROM_Get_64_Bit_Data_Address
      10. 5.2.10 EEPROM_Program_64_Bits
      11. 5.2.11 EEPROM_CheckStatus
      12. 5.2.12 ClearFSMStatus
    3. 5.3 Testing Example
  8. Single-Unit Emulation
    1. 6.1 User-Configuration
      1. 6.1.1 EEPROM_Config.h
      2. 6.1.2 F28P65x_EEPROM.c
    2. 6.2 EEPROM Functions
      1. 6.2.1  EEPROM_Config_Check
      2. 6.2.2  Configure_Protection_Masks
      3. 6.2.3  EEPROM_Write
      4. 6.2.4  EEPROM_Erase
      5. 6.2.5  EEPROM_GetValidBank
      6. 6.2.6  EEPROM_Get_64_Bit_Data_Address
      7. 6.2.7  EEPROM_UpdateBankStatus
      8. 6.2.8  EEPROM_UpdatePageStatus
      9. 6.2.9  EEPROM_Get_64_Bit_Data_Address
      10. 6.2.10 EEPROM_Program_64_Bits
      11. 6.2.11 EEPROM_CheckStatus
      12. 6.2.12 ClearFSMStatus
    3. 6.3 Testing Example
  9. Application Integration
  10. Adapting to Other Gen 3 C2000 MCUs
  11. Flash API
    1. 9.1 Flash API Checklist
      1. 9.1.1 Flash API Do's and Do Not's
  12. 10Source File Listing
  13. 11Conclusion
  14. 12References

EEPROM_Get_64_Bit_Data_Address

The EEPROM_Get_64_Bit_Data_Address() provides functionality for determining if the EEPROM unit is full and assigning the proper address, if required. If a full EEPROM unit is detected, EEPROM is erased using the EEPROM_Erase() function and the active EEPROM unit is switched.

First, the end address of EEPROM is set according to the device being used and the configuration. The END_OF_SECTOR directive is set in the EEPROM_Config.h file.

End_Address = (uint16 *)END_OF_SECTOR;  // Set End_Address for sector

Next, the EEPROM bank pointer is compared to the end address. If writing four 16-bit words beginning at the current EEPROM bank pointer would go beyond the end address, this indicates the sector is full. At this point, the active EEPROM unit is switched, new Write/Protection masks are configured, the Erase_Inactive_Unit flag is set, and the EEPROM EEPROM Bank Pointer is reset to the beginning of the newly active EEPROM unit.

if(Bank_Pointer > End_Address-3)         // Test if EEPROM is full
{
    EEPROM_ACTIVE_UNIT ^= 1; 

    uint64 WE_Protection_AB_Mask = Configure_Protection_Masks(
                                       FIRST_AND_LAST_SECTOR[EEPROM_ACTIVE_UNIT],
                                              NUM_EEPROM_SECTORS);


    WE_Protection_A_Mask = 0xFFFFFFFF ^ (uint32)WE_Protection_AB_Mask;
    WE_Protection_B_Mask = 0x00000FFF ^ WE_Protection_AB_Mask >> 32;

    Erase_Inactive_Unit = 1; 
    RESET_BANK_POINTER;  
}