SPRADE8 November   2023 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   EEPROM Emulation for Generation 3 C2000 Real Time Controllers
  2.   Trademarks
  3. Introduction
  4. Difference Between EEPROM and On-Chip Flash
  5. Overview
    1. 3.1 Basic Concept
    2. 3.2 Single-Unit Method
    3. 3.3 Ping-Pong Method
    4. 3.4 Creating EEPROM Sections (Pages) and Page Identification
  6. Software Description
    1. 4.1 Software Functionality and Flow
  7. Ping-Pong Emulation
    1. 5.1 User-Configuration
      1. 5.1.1 EEPROM_Config.h
      2. 5.1.2 F28P65x_EEPROM.c
    2. 5.2 EEPROM Functions
      1. 5.2.1  EEPROM_Config_Check
      2. 5.2.2  Configure_Protection_Masks
      3. 5.2.3  EEPROM_Write
      4. 5.2.4  EEPROM_Read
      5. 5.2.5  EEPROM_Erase
        1. 5.2.5.1 Erase_Bank
      6. 5.2.6  EEPROM_GetValidBank
      7. 5.2.7  EEPROM_UpdateBankStatus
      8. 5.2.8  EEPROM_UpdatePageStatus
      9. 5.2.9  EEPROM_Get_64_Bit_Data_Address
      10. 5.2.10 EEPROM_Program_64_Bits
      11. 5.2.11 EEPROM_CheckStatus
      12. 5.2.12 ClearFSMStatus
    3. 5.3 Testing Example
  8. Single-Unit Emulation
    1. 6.1 User-Configuration
      1. 6.1.1 EEPROM_Config.h
      2. 6.1.2 F28P65x_EEPROM.c
    2. 6.2 EEPROM Functions
      1. 6.2.1  EEPROM_Config_Check
      2. 6.2.2  Configure_Protection_Masks
      3. 6.2.3  EEPROM_Write
      4. 6.2.4  EEPROM_Erase
      5. 6.2.5  EEPROM_GetValidBank
      6. 6.2.6  EEPROM_Get_64_Bit_Data_Address
      7. 6.2.7  EEPROM_UpdateBankStatus
      8. 6.2.8  EEPROM_UpdatePageStatus
      9. 6.2.9  EEPROM_Get_64_Bit_Data_Address
      10. 6.2.10 EEPROM_Program_64_Bits
      11. 6.2.11 EEPROM_CheckStatus
      12. 6.2.12 ClearFSMStatus
    3. 6.3 Testing Example
  9. Application Integration
  10. Adapting to Other Gen 3 C2000 MCUs
  11. Flash API
    1. 9.1 Flash API Checklist
      1. 9.1.1 Flash API Do's and Do Not's
  12. 10Source File Listing
  13. 11Conclusion
  14. 12References

Testing Example

The examples provided were tested with F28P650DK9. To properly test the example, the memory window and breakpoints need to be utilized within Code Composer Studio. The following steps were followed to program and test the project.

  1. Connect the F28P650DK9 to the PC via USB and an XDS110 Debug Probe with JTAG connection.
  2. Connect a 5V DC power supply to the board.
  3. Start Code Composer Studio and open the F28P65x_EEPROM_PingPong_Example.pjt.
  4. Build the project by selecting Project -> Build Project.
  5. Launch the Target Configurations by going to View -> Target Configurations -> F28P65x_EEPROM_Example -> targetConfigs -> right-click TMS320F28P650DK9.ccxml -> Launch Selected Configuration.
  6. Connect to CPU1 by going to the Debug window, right clicking Texas Instruments XDS110 USB Debug Probe_0/C28xx_CPU1, and selecting Connect Target.
  7. Load symbols by clicking Load Symbols and selecting the F28P65x_EEPROM_PingPong.out from the project.
  8. Set breakpoints to properly view data written to and read from the memory within the memory window as shown in Break Points.
    GUID-20231017-SS0I-XJ66-XQW8-9T79XLFFLHKH-low.png Figure 6-2 Break Points
  9. Run to the first breakpoint and open the Memory Browser (View -> Memory Browser) to view the data. Bank_Pointer can be used to watch the data written and Read_Buffer to watch the data being read back from the memory. This is shown in Write to EEPROM and Read Data.
    GUID-20231017-SS0I-VQBK-W5MF-WSZTPPBMZZVW-low.png Figure 6-3 Write to EEPROM
    GUID-20231017-SS0I-7RCG-PH5K-FWRZCPG5PVTH-low.png Figure 6-4 Read Data
  10. Continue running from breakpoint to breakpoint until the program has finished or EEPROM is full.
  11. Once EEPROM is full, you will see the new data written to the previously inactive unit and the full EEEPROM will be erased. Shown in Erase full EEPROM Unit and Write to EEPROM.
    GUID-20231017-SS0I-LG3D-8THQ-JF5RDQGJRWF6-low.png Figure 6-5 Erase full EEPROM Unit
    GUID-20231017-SS0I-CG8Z-VBHS-JDW32JNZDX4V-low.png Figure 6-6 Write to EEPROM
  12. This process can be repeated as necessary.

The preceding steps were used to test the Page Mode configuration. The 64-Bit Mode configuration can also be tested with the same procedure. To enable 64-Bit Mode, change the definition in the EEPROM_Config.h file by un-commenting the _64_BIT_MODE directive and commenting out the PAGE_MODE directive.