SLVUBY7A October 2020 – October 2022 DRA821U , LP8764-Q1 , TPS6594-Q1
The C and D triggers, defined by the NSLEEPx bits or pins, trigger the TO_RETENTION sequence. This sequence disables all power rails and GPIOs that are not supply the retention rails. The sequence can by modified using the I2C_6 and I2C_7 bits found in the FSM_I2C_TRIGGERS register. These bits need to be set by I2C in both PMICs before a trigger for the retention state occurs. If the I2C_6 bit is set high in both PMICs, they will enter GPIO retention state as shown in Figure 6-14. If the I2C_7 bit is set high in both PMICs, they will enter DDR retention state as shown in Figure 6-15. If both bits are set, both GPIO and DDR rail will be retained, as shown in Figure 6-16. If neither I2C_6 or I2C_7 are set high, the GPIOs and DDR will not remain active, as shown in Figure 6-17.