SLVUBY7A October 2020 – October 2022 DRA821U , LP8764-Q1 , TPS6594-Q1
For ASIL-C or ASIL-D systems, there are additional features to the ones described in Section 4.1 that can be utilized. These features include:
The current monitoring is enabled by default for all BUCKs and LDOs for the TPS6594-Q1 and LP8764-Q1 devices. Additionally, Figure 3-1 shows that the MCU domain of the processor is powered by different power resources of the PMICs than the main power domain of the processor. SoC reset functionality is supported through the connection of GPIO_11 on TPS6594-Q1, configured as nRSTOUT_SoC, to the PORz pin of the processor.