SLLA651 April 2025 TCAN2845-Q1 , TCAN2847-Q1 , TCAN2855-Q1 , TCAN2857-Q1
VSUP is the main power supply input into the device. This pin needs to be connected to the main power supply of the system – which is generally a battery that is nominally at a 12V output. This pin needs to have a reverse polarity protection diode between the pin and the power source as well as decoupling capacitances – especially a 100nF high frequency decoupling capacitor close to VSUP pin in addition to bulk capacitances. This is also highly suggested to include a PI filter after the diode that acts as an EMI filter. The SBC requires for operation that the VSUP voltage is between 5.5V to 28V which makes this a great option for 12V battery systems. The VSUP pin also acts as the input for the integrated LDOs as well as the external PNP attached to the integrated LDO controller. The voltage on VSUP governs when the device enters init and restart modes.