SLLA651 April 2025 TCAN2845-Q1 , TCAN2847-Q1 , TCAN2855-Q1 , TCAN2857-Q1
With a basic understanding of how the device transitions between the different operational states, this is crucial to understand the power electronics within the device as well as some of the limitations. The TCAN28XX devices can be thought of as having three distinct power inputs and four distinct power management subsystems that act as power outputs and three distinct power inputs. The power inputs are VSUP, VHSS, and VCAN. For the power outputs, there are two integrated LDOs (VCC1 and VCC2), one integrated LDO controller (VEXCC), and four high side switch modules (HSS1 – HSS4).