SLLA651 April 2025 TCAN2845-Q1 , TCAN2847-Q1 , TCAN2855-Q1 , TCAN2857-Q1
The last protection feature that has been briefly mentioned previously is the LIMP pin which supports LIMP home functionality. The LIMP signal is an active low output that can signal a system that there is a major issue that is occurring on the device. By default, the LIMP pin can activate when there are missed watchdog triggers and won’t reset until the configured condition is met - which by default is three correct watchdog triggers after the missed watchdog trigger. This pin also can activate when the device enters into fail-safe mode alerting the system at large that there was a fault that caused the SBC to enter the fail-safe mode. This is possible to read the LIMP pin state, assuming VCC1 is active, by first enabling the read ability, which is done by setting 1A[6] = 1, then reading the LIMP state at address 1A[5].