SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The Host driver writes the boot timeout value into MMCSD0_BOOT_TIMEOUT_CONTROL register as per the eMMC4.3+ spec.
When the Host driver sets the "BOOT_ENABLE" to 1 in MMCSD0_BLOCK_GAP_CONTROL register and "DATA_XFER_DIR" bit to "1" in MMCSD0_TRANSFER_MODE register, the Host controller drives the CMD line to "0" for boot operation.
If the Host controller is configured to wait for boot acknowledgement from the eMMC4.3+ device, the controller receives the boot acknowledgement and asserts the "RCV_BOOT_ACK" interrupt to the driver (MMCSD0_NORMAL_INTR_STS[13] RCV_BOOT_ACK). If the Host controller doesn't receive the boot acknowledgement from the device within the timeout value, the Host controller will assert the data timeout error interrupt (MMCSD0_ERROR_INTR_STS[4] DATA_TIMEOUT).
After servicing the boot acknowledge interrupt or data timeout error interrupt, the driver programs the MMCSD0_BOOT_TIMEOUT_CONTROL register with boot data timeout value.
The eMMC4.3+ device starts sending the boot data on the data line and Host controller sends the same to system whenever a block of data is received from device. The Host controller terminates the boot operation when the programmed number of blocks is transferred to the System. The Driver can writes "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register.
The boot operation can also be terminated in between the boot transfer (the Driver can set the "BOOT_ENABLE" as "0" anytime to disable the boot operation). After the boot termination, the Host controller asserts soft reset for CMD line and DATA line internally once the driver clears the BOOT_COMPLETE interrupt (MMCSD0_NORMAL_INTR_STS[14] BOOT_COMPLETE), to reset all the state machines to idle state.
There is no need to perform error recovery sequence in case data timeout interrupt occurs during boot operation (ignore sending abort command, soft reset and just clear the timeout interrupt and proceed with the boot flow).
If the device sends wrong acknowledgement to the Host, the Host controller will assert Data CRC Error interrupt (MMCSD0_ERROR_INTR_STS[5] DATA_CRC) on the Driver. In this case, the Host driver has to stop the boot mode operation by setting "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register and write soft reset for CMD and data line.
If the device sends end bit as "0" in acknowledgement to the Host, the Host controller will assert Data End Bit Error interrupt (MMCSD0_ERROR_INTR_STS[6] DATA_ENDBIT) on the Driver.
The Host driver stops the boot mode operation by setting "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register and write soft reset for CMD and data line.
Note: Enable the MMCSD0_BLOCK_GAP_CONTROL[7] BOOT_ACK_ENA bit during boot operation. If failed, the controller will not wait for boot acknowledge from the card and send out data CRC error when the card sends boot acknowledgement first and followed by boot data.