SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The DSITX controller can be configured to perform a transition between LP state and HS state during the horizontal lines which have long periods of blanking. The registers controlling the timing for the DPHY wakeup time and the reg_line_duration must be programmed to exactly match the DPI cycles of the horizontal line to the tx_byte_clk cycles required for the number of active lanes selected.
The LP operation for each vertical blanking line will require the reg_line_duration to be configured to match the following:
Note REG_WAKEUP_TIME is used internally to adjust the cycles for each vertical LP line.