SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The Rx PSI-L Interface master may assert the rstrmp_drop signal co-incident with the transfer of any data phase of a packet. When this signal is sampled asserted by the UDMA, the drop condition will be latched into a flag for that thread and the Rx Packet DMA unit will be notified that the packet is to be flushed and recycled rather than passed to the host. The drop signal is only required to be asserted with a single data phase and will only cause the current packet to be dropped from packet stream. The UDMA will drop all data given to it until the EOP is found on the thread and then the internal drop flag will be cleared. When the UDMA drops a packet on a channel configured for Packet mode there is no notification to the host.