ZHCSI27C April 2018 – October 2021 LM5036
PRODUCTION DATA
The voltage applied to the VIN pin of LM5036 device serves as the input voltage for the internal VCC startup regulator and auxiliary supply. In typical applications, the VIN pin voltage is the same as the input voltage for the main half-bridge converter. The recommended range of the VIN pin voltage is 18-V to 100-V. Figure 8-2 shows the recommended filter to suppress transients that may occur at the input supply. This suppression is particularly important when the input voltage rises to a level near the maximum recommended operating rating (100-V) of the LM5036 device.