TIDUE59A May 2018 – September 2020
The OTA library used in this example implements a simple HyperText Transfer Protocol (HTTP) client, which supports the Dropbox API and can be used to download the software update. The source for the simple HTTP client implementation is in the OtaHttpClient.h/.c files of the OTA library. For additional details on the implementation of the cloud OTA solution used in this design and the SimpleLink OTA library, see the SimpleLink Academy Training on Wi-Fi OTA.