TIDUE59A May 2018 – September 2020
Table 3-7 shows the set of pass or fail tests that were used to evaluate the performance of the TIDC-01005. All tests were performed using the software provided with the TIDC-01005 and the hardware setup described in Section 3.1.
| TEST DESCRIPTION | RESULT |
|---|---|
| Provision system to a new Wi-Fi network using AP provisioning | Pass |
| Provision system to a new Wi-Fi network using TI SmartConfig | Pass |
| Provision system to a new Wi-Fi network using BLE Provisioning | Pass |
| System automatically connects to a stored profile out of reset/hibernate if it exists | Pass |
| System connects to MQTT broker over TLS with server authentication | Pass |
| System receives lock and unlock commands from the cloud and drives the motor appropriately | Pass |
| System sends lock status to the cloud when polled by the user | Pass |
| System software successfully updates using a cloud-based OTA software update | Pass |