ZHCSA18F March 2009 – February 2021 TMS320C28341 , TMS320C28342 , TMS320C28343 , TMS320C28343-Q1 , TMS320C28344 , TMS320C28345 , TMS320C28346 , TMS320C28346-Q1
PRODUCTION DATA
Figure 8-28 shows the OSC and PLL block.
Figure 8-28 OSC and PLL Block DiagramThe on-chip oscillator circuit enables a crystal/resonator to be attached to the C2834x devices using the X1 and X2 pins. If the on-chip oscillator is not used, an external oscillator can be used in either one of the following configurations:
The three possible input-clock configurations are shown in Figure 8-29 to Figure 8-31.
Figure 8-29 Using a 3.3-V External Oscillator
Figure 8-30 Using a 1.8-V External Oscillator
Figure 8-31 Using the Internal Oscillator