ZHCSR35A November 2019 – August 2020 BQ79600-Q1
PRODUCTION DATA
In ACTIVE mode, stack devices can embed their fault status in their response frames (refer to Figure 7-7) that are sent to BQ79600-Q1. The BQ79600-Q1 can detect their embedded fault info and sets [FTONE_DET] bit once criteria in Figure 7-25 is met. Please refer to BQ7961X-Q1 on how to use embeded fault feature.
To pass on the fault status of the stack devices, the host sends a stack read which will result with response frame pass through every device in the daisy chain, giving each device an opportunity to embed their fault status to response frame.
Figure 7-25 Embed Fault Detection in
Response Frame