ZHCSK66C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
Read-data-continuous mode is stopped by the SDATAC command and put into read-data-by-command mode. In read-data-by-command mode, an RDATA command must be sent to the device for each data conversion (as shown in Figure 54). When the read data command is received (on the eighth SCLK rising edge), data are available to read only when DRDY goes low (tDR). When DRDY goes low, conversion data appear on DOUT. The data may be read on the rising edge of SCLK.
PARAMETER | DESCRIPTION | MIN | TYP | MAX | UNIT |
---|---|---|---|---|---|
tDR | Time for new data after data read command | 0 | 1 | fDATA |