ZHCSK66C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
The minimum phase filter provides a short delay from the arrival of an input signal to the output, but the relationship (phase) is not constant versus frequency, as shown in Figure 42. The filter phase is selected by the PHS bit, as Table 10 shows.
PHS BIT | FILTER PHASE |
---|---|
0 | Linear |
1 | Minimum |