ZHCSK66C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
The last stage of the ADS1283 filter block is a first-order HPF implemented as an IIR structure. This filter stage blocks dc signals, and rolls off low-frequency components below the cutoff frequency. The transfer function for the filter is shown in Equation 11:
where
The high-pass corner frequency is programmed by registers HPF[1:0], in hexadecimal. Equation 13 is used to set the high-pass corner frequency. Table 11 lists example values for the high-pass filter.
where
fHP (Hz) | DATA RATE (SPS) | HPF[1:0] |
---|---|---|
0.5 | 250 | 0337h |
1.0 | 500 | 0337h |
1.0 | 1000 | 019Ah |
The HPF causes a small gain error, in which case the magnitude of the error depends on the ratio of fHP / fDATA. For many common values of (fHP / fDATA), the gain error is negligible. Figure 43 shows the gain error of the HPF.
The gain error factor is illustrated in Equation 14:
Figure 44 shows the first-order amplitude and phase response of the HPF. In the case of applying step inputs or synchronizing, make sure to take the settling time of the filter into account.