ZHCSK66C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
The serial interface is reset each time CS is taken high. However, for applications that tie CS low, the serial port cannot be reset by taking CS high; reset of the serial interface is no longer possible by using CS. The ADS1283 provides a feature that automatically recovers the interface when a transmission is stopped or interrupted, or if an inadvertent glitch appears on SCLK. To reset the serial interface, hold SCLK low for 64 DRDY cycles. The reset of the serial interface results in termination of data transfer or commands in progress. After serial port reset occurs, the next SCLK pulse starts a new communication cycle. To prevent automatic reset from occurring, pulse SCLK at least once for every 64 DRDY pulses.