SWRU612B December   2023  – June 2026 CC3300 , CC3300MOD , CC3301 , CC3301MOD , CC3351 , CC3351MOD

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Overview
  5. 2Schematic Considerations – CC33xx Devices
    1. 2.1 Schematic Reference Design
    2. 2.2 Power Supply
      1. 2.2.1 Power Input/Output Requirements
      2. 2.2.2 Boot Sequence
        1. 2.2.2.1 SOP Modes
      3. 2.2.3 Power Down Sequence
    3. 2.3 Clock Source
      1. 2.3.1 Fast Clock
      2. 2.3.2 Slow Clock
        1. 2.3.2.1 Slow Clock Generated Internally
        2. 2.3.2.2 Slow Clock Using an External Oscillator
    4. 2.4 Radio Frequency (RF)
    5. 2.5 Digital Interfaces
      1. 2.5.1 Reset
      2. 2.5.2 Secure Digital Input Output (SDIO)
        1. 2.5.2.1 SDIO Timing Diagram: Default Speed
        2. 2.5.2.2 SDIO Timing Diagram: High Speed
      3. 2.5.3 Serial Peripheral Interface (SPI)
        1. 2.5.3.1 SPI Timing Diagram
      4. 2.5.4 Universal Asynchronous Receiver-Transmitter (UART)
        1. 2.5.4.1 UART Timing Diagram
      5. 2.5.5 Serial Wire Debug (SWD)
      6. 2.5.6 WLAN Interrupt Request (HOST_IRQ_WL)
      7. 2.5.7 Logger
      8. 2.5.8 Coexistence
  6. 3Layout Considerations – CC33xx Devices
    1. 3.1 Layout Reference Design
      1. 3.1.1 Reference Design – CC330x Single Band Layout
      2. 3.1.2 Reference Design – CC335x Dual Band Layout
      3. 3.1.3 BP-CC3351 Design Layout
      4. 3.1.4 M2-CC3351 Design Layout
    2. 3.2 IC Thermal Pad
    3. 3.3 Radio Frequency (RF)
    4. 3.4 XTAL
    5. 3.5 Power Supplies
    6. 3.6 SDIO
  7. 4Schematic Considerations – CC33xxMOD
    1. 4.1 Schematic Reference Design – CC33xxMOD
    2. 4.2 Power Supply
  8. 5Layout Considerations – CC33xxMOD
    1. 5.1 CC33xxMOD RF Layout Recommendations
  9. 6 CC33xxMOD Regulatory Compliance
    1. 6.1 CC33xxMOD OEM Integration Manual
  10. 7Revision History

Power Supplies

The power supplies, ground traces, and decoupling capacitors are important for improving layout. Since the decoupling capacitors can be close to the RF pins and traces of the device and power supplies, traces must be thick enough to support the necessary current to the device.

  • PA_LDO_OUT (pin 1): TI suggests placing the decoupling capacitor close to the device pin and having a thick enough trace to have a low impedance path to the capacitor. See Figure 3-16 for a visual representation.
  • VDDA_IN1 and VDDA_IN2 (pins 4 and 5): The supply side of the decoupling capacitors must be shorted together with a polygon region with two power vias (one for each decoupling capacitor). The ground side of each capacitor must go directly to ground by separate vias (not shorted together) and be isolated from the rest of the ground plane on the top layer.
  • For the 1.8V power delivery, a thick trace or power plane must be used to carry the required amount of current consumption in the VDD_MAIN_IN, VIO, VDDA_IN1, VDDA_IN2, and VPP_IN pins combined. See Table 4-9 for maximum current consumption.
  • The 1.8V path must be located around the device on a layer that is not the top layer or ground layer (place the path on layer 3 or 4). This way, the power path cannot interrupt the RF trace on the top layer (layer 1) or the continuous ground layer (layer 2). Only one via is used for each 1.8V power supply. The 1.8V supply currents must not flow under the device.
  • For the 3.3V power delivery, a thick trace or a power plane must be used to carry the required amount of current consumption of the PA_LDO_IN pins. See Table 4-9 for more information. The power delivery must also be placed on a layer that is not the top layer or ground layer (layer 3 or 4).
  • PA_LDO_IN (pins 39 and 40): These two pins must be shorted together with a solid region. The decoupling capacitor must be placed close to the device. Use two vias (if possible) to deliver the 3.3V rail.
  • The ground for pins 37 and 38 must be shorted together with a solid region. This solid region must be connected to the thermal ground pad of the device.
  • The ground for pin 3 must be shorted to the thermal pad under the device and to the ground plane that is adjacent to the RF trace.

Figure 3-16 is sampled from the BP-CC3351 design files.

M2-CC3351 CC3351MOD CC3351 CC3301MOD CC3301 CC3300MOD CC3300 BP-CC3351 Reference Layout of CC33xx Power Supplies Figure 3-16 Reference Layout of CC33xx Power Supplies

Figure 3-17 is sampled from the M2-CC3351 design files.

M2-CC3351 CC3351MOD CC3351 CC3301MOD CC3301 CC3300MOD CC3300 BP-CC3351 Reference Layout of the Power
                    Layer Figure 3-17 Reference Layout of the Power Layer