SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
If the McBSP is unused (the serial port transmit and receive sections are reset), the companding hardware can compand internal data. This can be used to:
Figure 20-6 shows two methods by which the McBSP can compand internal data. Data paths for these two methods are used to indicate:
The advantage of this method is the speed. The disadvantage is that there is no synchronization available to the CPU and DMA to control the flow. DRR1 and DXR1 are internally connected if the (X/R)COMPAND bits are set to 10b or 11b (compand using μ-law or A-law).
Figure 20-6 Two Methods by Which the McBSP
Can Compand Internal Data