SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
One of the simplest power converter topologies is the buck. A single ePWM module configured as a master can control two buck stages with the same PWM frequency. If independent frequency control is required for each buck converter, then one ePWM module must be allocated for each converter stage. Figure 14-61 shows four buck stages, each running at independent frequencies. In this case, all four ePWM modules are configured as Masters and no synchronization is used. Figure 14-62 shows the waveforms generated by the setup shown in Figure 14-61; note that only three waveforms are shown, although there are four stages.
Figure 14-62 Buck Waveforms for Control of Four Buck Stages (Note: Only three bucks shown here)