SPRK066 October 2025 F28377D-SEP
The heavy-ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For these studies, ion flux of 104-105 ions×cm2/s were used to provide heavy-ion fluences of 106-107 ions×cm2/s
For the experiments conducted on this report, there were 2 ions used, 109Ag and 40Ar. 109Ag was used to obtain LETEFF of 45MeV·cm2/mg. 40Ar was used to obtain LETEFF of 8MeV·cm2/mg. The total kinetic energys for each of the ions were:
109Ag = 1.27 GeV (15MeV/nucleon)
Ion uniformity for these experiments was on average 91%
40Ar = 536.9MeV (15MeV/nucleon)
Ion uniformity for these experiments was on average 94%
Figure 4-1 shows the F28377D EVM used for the data collection at the TAMU facility. Although not visible in this photo, the beam port has a 1-mil Aramica window to allow in-air testing while maintaining the vacuum within the accelerator with only minor ion energy loss. The in-air gap between the device and the ion beam port window was maintained at 40mm for all runs.
Figure 4-1 Photograph of the F28377D-SEP EVM in
Front of the Heavy-Ion Beam Exit Port at the Texas A&M Cyclotron