SPRADP4 February   2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1 , AM67 , AM68A , AM69A , DRA821U , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VM-Q1 , TDA4VP-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2MCAN Features
  6. 3MCAN Software Configuration
    1. 3.1 Filter Configuration
    2. 3.2 Transmitter Delay Compensation
    3. 3.3 MCAN Bit Timing Parameters
  7. 4Debug Tips to Resolve MCAN Communication Issues
    1. 4.1 Debugging the MCAN Hardware
    2. 4.2 Debugging using MCAN registers
      1. 4.2.1 MCAN Protocol Status Register
      2. 4.2.2 MCAN Error Counter Register
    3. 4.3 Understanding MCAN applications in TI SDKs
      1. 4.3.1 MCU PLUS SDK
      2. 4.3.2 Linux SDK
      3. 4.3.3 MCAL SDK
      4. 4.3.4 PDK
    4. 4.4 Other Common Issues
  8. 5Related FAQs
  9. 6Summary
  10. 7References

Debug Tips to Resolve MCAN Communication Issues

CAN controllers have an on-chip error detection mechanism. If any node detects an error at the time of transmission or reception of a message, then the discovering node transmits an error flag or error frame. This helps in detection of faulty CAN frames. The other nodes also detect the error caused by the error flag if the nodes failed to detected the original error. This helps in taking appropriate action in rejection of that message.