ZHCSMX7A August 2021 – December 2021 TPS92519-Q1
PRODUCTION DATA
The TPS92519-Q1 uses an adaptive on-time control scheme and does not have a dedicated on-board oscillator. The one-shot timer is programmed by the voltage on FSET input. The on-time is calculated internally using Equation 1 and is inversely proportional to the measured input voltage, VIN, and proportional to the measured CSP voltage, VCSP.

Constant, κ, is set by the FSET pin logic.

Given the duty ratio of the buck converter is VCSP / VIN, the switching period, TSW, remains nearly constant over all operating points. Use Equation 3 to calculate the switching period.

Use Equation 4 to calculate the switching frequency.