ZHCSMU5A July 2020 – December 2020 TPS25814
PRODUCTION DATA
Top and bottom placement is used for this example to minimize solution size. The TPS25814 is placed on the top side of the board and the majority of its components are placed on the bottom side. When placing the components on the bottom side, it is recommended that they are placed directly under the TPS25814. When placing the VBUS and PPHV capacitors it is easiest to place them with the GND terminal of the capacitors to face outward from the TPS25814 or to the side since the drain connection pads on the bottom layer should not be connected to anything and left floating. All other components that are for pins on the GND pad side of the TPS25814 should be placed where the GND terminal is underneath the GND pad.
The CC capacitors should be placed on the same side as the TPS25814 close to the respective CC1 and CC2 pins. Do NOT via to another layer in between the CC pins to the CC capacitor, placing a via after the CC capacitor is recommended.
The ADCIN1/2 voltage divider resistors can be placed where convenient.
The figures below show the placement in 2-D and 3-D.