ZHCSOU1 February 2023 DS90UB638-Q1
PRODUCTION DATA
BIT | FIELD | TYPE | DEFAULT | DESCRIPTION |
---|---|---|---|---|
7:6 | RESERVED | RW | 0x0 | RESERVED |
5 | DISCARD_ON _PAR_ERR | RW | 1 | Discard frames on Parity Error 0 : Forward packets with parity errors 1 : Truncate Frames if a parity error is detected |
4 | DISCARD_ON _LINE_SIZE | RW | 0 | Discard frames on Line Size 0 : Allow changes in Line Size within packets 1 : Truncate Frames if a change in line size is detected |
3 | DISCARD_ON _FRAME_SIZE | RW | 0 | Discard frames on change in Frame Size When enabled, a change in the number of lines in a frame will result in truncation of the packet. The device will resume forwarding video frames based on the PASS_THRESHOLD setting in the PORT_PASS_CTL register. 0 : Allow changes in Frame Size 1 : Truncate Frames if a change in frame size is detected |
2 | RESERVED | RW | 0 | Reserved |
1 | RESERVED | RW | 0 | Reserved |
0 | RESERVED | RW | 0 | Reserved |