SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The operation of the RTI module is guaranteed in run, doze and snooze mode. In sleep or hibernate mode all clocks will be switched off and the RTI module will not work.
In doze and snooze modes all parts of the RTI are active, since it has to be able to wake up the device with compare and timebases interrupts. Capturing events generated by the interrupt module is also possible since in both modes the peripheral modules are able to generate interrupts, which can trigger capture events. The RTI module will generate compare and timebases interrupts. The compare interrupts will periodically wake up the device.
In the special case of doze mode with DPLL off, RTI_FCLK might have a different period than with DPLL enabled, since RTI_FCLK will be derived from the oscillator output. It has to be ensured that the RTI_ICLK to RTI_FCLK ratio is at least 3:1.
The DWD/DWWD remains active when the device enters low power mode as long as the RTI_FCLK is kept active.
Whenever the LPSC that controls an RTI is in any state other than Enable (see Module States), the RTI cannot count or generate interrupts. For more information, see Power Control Modules.
During standard SoC warm reset the RTI and the rest of the SoC are reset. In this case, the RTI counters are stopped and interrupts are not issued. During reset-isolated warm reset, if an R5FSS is put in reset-isolation, then the associated RTI also becomes reset isolated. As such, the R5FSS and the RTI are not reset, but RTI stops counting and cannot generate interrupts until R5FSS is taken out of CLKSTOP (brought to Enable state).