SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
If the system determines that it needs to flush all outstanding transactions (for instance, because the main SoC is in an error condition and is going to be reset), software may do this by writing to the Flush Register (Base Address + 0x10). Once all transactions are flushed, software should exit Flush mode. If the destination side is in reset, this should trigger hardware flush, keeping the gasket returning any transactions that arrive. The system should keep transactions from going to the gasket when the destination side is taken down as well.