SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The timing of Stop At Block Gap Request and Continue Request. The Transfer Complete interrupt (MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE) is always generated by setting MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit where data transfer is stopped. However, generation of the Block Gap Event interrupt (MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT) is dependent on whether the last data block is sent or not. Block Gap Event is not generated If all data blocks are transferred (the last block is transferred). It is not necessary to enable Block Gap Event interrupt. The status can be checked when transfer complete interrupt is detected. It is not necessary to use Continue Request (MMCSD0_BLOCK_GAP_CONTROL[1] CONTINUE) if Block Gap Event status is not set because there is no further data to be transferred. If Read Wait is not supported, Host Controller stops SD Clock at the block gap.
Implementation Note:
The MMCSD0_BLOCK_GAP_CONTROL[2] RDWAIT_CTRL, MMCSD0_PRESENTSTATE[2] DATA_LINE_ACTIVE, MMCSD0_PRESENTSTATE[9] RD_XFER_ACTIVE bits shall be set and cleared by the Host Controller.
The MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit shall be set and cleared by the Host Driver. The MMCSD0_BLOCK_GAP_CONTROL[1] CONTINUE bit shall be set by the Host Driver and be cleared by the Host Controller. The MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT bit and MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE bit shall be set by the Host Controller and be cleared by the Host Driver.
Figure 12-149 Wait Read Transfer by Stop At Block Gap RequestThe Host Controller can accept a Stop At Block Gap Request (MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP) when all the following conditions are met.
(1) It is at the block gap.
(2) The Host Controller can assert read wait or it is already asserted.
(3) The MMCSD0_BLOCK_GAP_CONTROL[2] RDWAIT_CTRL bit is set to 1.
After accepting the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit:
(1) Clear MMCSD0_PRESENTSTATE[2] DATA_LINE_ACTIVE bit and generate the Block Gap Event Interrupt (MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT).
(2) After all valid data has been read (No valid read data remains in the Host Controller), clear the MMCSD0_PRESENTSTATE[9] RD_XFER_ACTIVE bit and generate the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE).
(3) After accepting MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE bit, clear the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit.
Figure 12-150 Stop At Block Gap Request is Not Accepted at the Last Block of the Read TransferIf the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit is set to 1 during the last block transfer, the Host Controller shall not accept the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit and stops the transaction normally. The Block Gap Event Interrupt (MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT) is not generated. When the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE) is generated, and if the MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT bit status is not set to 1, the driver shall clear the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit.
Figure 12-151 Continue Read Transfer by Continue RequestTo restart a stopped data transfer, set the MMCSD0_BLOCK_GAP_CONTROL[1] CONTINUE bit to 1 (the MMCSD0_BLOCK_GAP_CONTROL[0] STOP_AT_BLK_GAP bit shall be set to 0).
After accepting the MMCSD0_BLOCK_GAP_CONTROL[1] CONTINUE bit:
(1) Release MMCSD0_BLOCK_GAP_CONTROL[2] RDWAIT_CTRL bit (if the data block can accept the next data).
(2) Set the MMCSD0_PRESENTSTATE[2] DATA_LINE_ACTIVE bit and the MMCSD0_PRESENTSTATE[9] RD_XFER_ACTIVE bit.
(3) The MMCSD0_BLOCK_GAP_CONTROL[1] CONTINUE bit is automatically cleared by (2).
The end of the read transfer is specified by data length.
(1) Clear the MMCSD0_PRESENTSTATE[2] DATA_LINE_ACTIVE bit and do not generate the Block Gap Event Interrupt (MMCSD0_NORMAL_INTR_STS[2] BLK_GAP_EVENT bit).
(2) After all valid data has been read (No valid read data remains in the Host Controller), clear the MMCSD0_PRESENTSTATE[9] RD_XFER_ACTIVE bit and generate the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS[1] XFER_COMPLETE bit).