SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from eCAP, X-Bar or EPWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 4-13. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 21-8.
Figure 21-7 Details of the Counter and
Synchronization Block
Figure 21-8 eCAP
Synchronization Scheme