SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Figure 11-8 shows the EMIF's external pins used in interfacing with an asynchronous device. In EM1CS[n], n = 2, 3, or 4.
Figure 11-8 EMIF Asynchronous InterfaceOf special note is the connection between the EMIF and the external device's address bus. The EMIF address pin EM1A[0] always provides the least-significant bit of a 32-bit word address. Therefore, when interfacing to a 16-bit or 8-bit asynchronous device, the EM1BA[1] and EM1BA[0] pins provide the least-significant bits of the halfword or byte address, respectively. Figure 11-9 and Figure 11-10 show the mapping between the EMIF and the connected device's data and address pins for various programmed data bus widths. The data bus width can be configured in the asynchronous n configuration register (ASYNC_CSn_CR).
Figure 11-10 shows an interface between the EMIF and an external memory with byte enables. The EMIF must be operated in either normal mode or select strobe mode when using this interface, so that the EM1DQM signals operate as byte enables.
Figure 11-9 EMIF to 8-bit/16-bit Memory Interface
Figure 11-10 Common Asynchronous Interface