SPRUIZ1B July 2023 – August 2024
The UART peripheral includes an IrDA SIR encoder and decoder block. The IrDA SIR block provides functionality that converts between an asynchronous UART data stream and a half-duplex serial SIR interface. No analog processing is performed on-chip. The role of the SIR block is to provide a digital encoded output and decoded input to the UART. When enabled, the SIR block uses the UnTx and UnRx pins for the SIR protocol. These signals must be connected to an infrared transceiver to implement an IrDA SIR physical layer link. The SIR block can receive and transmit, but the SIR block is only half-duplex so the SIR block cannot do both at the same time. Transmission must be stopped before data can be received. The IrDA SIR physical layer specifies a minimum 10ms delay between transmission and reception. The SIR block has two modes of operation:
Whether the device is in normal or low-power IrDA mode, a start bit is deemed valid if the decoder is still low one period of IrLPBaud16 after the low was first detected. This enables a normal-mode UART to receive data from a low-power mode UART that can transmit pulses as small as 1.41µs. Thus, for both low-power and normal mode operation, the ILPDVSR field in the UARTILPR register must be programmed such that 1.42MHz < fIrLPBaud16< 2.12MHz, resulting in a low-power pulse duration of 1.41 to 2.11μs (three times the period of IrLPBaud16). The minimum frequency of IrLPBaud16 make sure that pulses less than one period of IrLPBaud16 are rejected, but pulses greater than 1.4μs are accepted as valid pulses.
Figure 36-3 shows the UART transmit and receive signals, with and without IrDA modulation.
Figure 36-3 IrDA Data ModulationIn both normal and low-power IrDA modes:
The IrDA SIR physical layer specifies a half-duplex communication link, with a minimum 10ms delay between transmission and reception. This delay must be generated by software because the delay is not automatically supported by the UART. The delay is required because the infrared receiver electronics can become biased or even saturated from the optical power coupled from the adjacent transmitter LED. This delay is known as latency or receiver setup time.