SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Table 8-63 lists the memory-mapped registers for the CLB_LOGIC_CONTROL_REGS registers. All register offset addresses not listed in Table 8-63 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | CLB_LOAD_EN | Global enable & indirect load enable control, only Global Enable Bit is LOCK protected | LOCK | Go |
| 2h | CLB_LOAD_ADDR | Indirect address | Go | |
| 4h | CLB_LOAD_DATA | Data for indirect loads | Go | |
| 6h | CLB_INPUT_FILTER | Input filter selection for both edge detection and synchronizers | LOCK | Go |
| 8h | CLB_IN_MUX_SEL_0 | Input selection to decide between Signals and GP register | LOCK | Go |
| Ah | CLB_LCL_MUX_SEL_1 | Input Mux selection for local mux | LOCK | Go |
| Ch | CLB_LCL_MUX_SEL_2 | Input Mux selection for local mux | LOCK | Go |
| Eh | CLB_BUF_PTR | PUSH and PULL pointers | Go | |
| 10h | CLB_GP_REG | General purpose register for CELL inputs | Go | |
| 12h | CLB_OUT_EN | CELL output enable register | Go | |
| 14h | CLB_GLBL_MUX_SEL_1 | Global Mux select for CELL inputs | LOCK | Go |
| 16h | CLB_GLBL_MUX_SEL_2 | Global Mux select for CELL inputs | LOCK | Go |
| 18h | CLB_PRESCALE_CTRL | Prescaler register control | LOCK | Go |
| 20h | CLB_INTR_TAG_REG | Interrupt Tag register | Go | |
| 22h | CLB_LOCK | Lock control register | EALLOW | Go |
| 24h | CLB_HLC_INSTR_READ_PTR | HLC instruction read pointer | Go | |
| 26h | CLB_HLC_INSTR_VALUE | HLC instruction read value | Go | |
| 2Eh | CLB_DBG_OUT_2 | Visibility for CLB inputs and final asynchronous outputs | Go | |
| 30h | CLB_DBG_R0 | R0 of High level Controller | Go | |
| 32h | CLB_DBG_R1 | R1 of High level Controller | Go | |
| 34h | CLB_DBG_R2 | R2 of High level Controller | Go | |
| 36h | CLB_DBG_R3 | R3 of High level Controller | Go | |
| 38h | CLB_DBG_C0 | Count of Unit 0 | Go | |
| 3Ah | CLB_DBG_C1 | Count of Unit 1 | Go | |
| 3Ch | CLB_DBG_C2 | Count of Unit 2 | Go | |
| 3Eh | CLB_DBG_OUT | Outputs of various units in the Cell | Go |
Complex bit access types are encoded to fit into small table cells. Table 8-64 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| R-1 | R -1 | Read Returns 1s |
| Write Type | ||
| W | W | Write |
| W1C | W 1C | Write 1 to clear |
| WSonce | W Sonce | Write Set once |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
CLB_LOAD_EN is shown in Figure 8-62 and described in Table 8-65.
Return to the Summary Table.
Global enable & indirect load enable control, only Global Enable Bit is LOCK protected
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PIPELINE_EN | NMI_EN | STOP | GLOBAL_EN | LOAD_EN | ||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-5 | RESERVED | R-0 | 0h | Reserved |
| 4 | PIPELINE_EN | R/W | 0h | This bit controls pipelining of all the CLB operations in HLC and Counter blocks. Pipelined operation is enabled when this bit is set to 1. Reset type: SYSRSn |
| 3 | NMI_EN | R/W | 0h | This bit controls the generation of NMI along with the interrupt whenever a INTR operation is executed by the HLC. NMI generation is disabled by default. It will be enabled when this bit is set to 1. Reset type: SYSRSn |
| 2 | STOP | R/W | 0h | This bit defines the behaviour of the sequential elements in the CELL during debug HALTs of the CPU. If this bit is set to 0, the debug HALT condition is ignored. Reset type: SYSRSn |
| 1 | GLOBAL_EN | R/W | 0h | This bit is a global enable signal for the logic in the CELL. This also acts as a soft reset for the CELL logic. CLB outputs (including LUTs and OUTLUTs) will be gated when this bit is cleared from 1 to 0, i.e., the CLB outputs will be low when GLOBAL_EN is low. Additionally, the FSM and AOC blocks will also be reset. Note that when this bit goes low, the COUNTER blocks and HLC are simply halted, but they will NOT be reset internally. This allows the ability to preload these submodules when GLOBAL_EN is 0. This bit is normally set after all the other configuration settings are completed. This bit is LOCK protected. Reset type: SYSRSn |
| 0 | LOAD_EN | R/W | 0h | A write with this bit set to 1 will pulse the Load Enable signal for the indirect register loads in the CELL. Reset type: SYSRSn |
CLB_LOAD_ADDR is shown in Figure 8-63 and described in Table 8-66.
Return to the Summary Table.
Indirect address
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ADDR | ||||||||||||||||||||||||||||||
| R-0-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-6 | RESERVED | R-0 | 0h | Reserved |
| 5-0 | ADDR | R/W | 0h | These are the address bits used for writing to the indirect address space of the CELL. Reset type: SYSRSn |
CLB_LOAD_DATA is shown in Figure 8-64 and described in Table 8-67.
Return to the Summary Table.
Data for indirect loads
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DATA | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DATA | R/W | 0h | This register holds the 32-bit data for writing to the indirect address space of the CELL. Reset type: SYSRSn |
CLB_INPUT_FILTER is shown in Figure 8-65 and described in Table 8-68.
Return to the Summary Table.
Input filter selection for both edge detection and synchronizers
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| PIPE7 | PIPE6 | PIPE5 | PIPE4 | PIPE3 | PIPE2 | PIPE1 | PIPE0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| SYNC7 | SYNC6 | SYNC5 | SYNC4 | SYNC3 | SYNC2 | SYNC1 | SYNC0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| FIN7 | FIN6 | FIN5 | FIN4 | ||||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| FIN3 | FIN2 | FIN1 | FIN0 | ||||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | PIPE7 | R/W | 0h | Enable pipelining for Input 7 Reset type: SYSRSn |
| 30 | PIPE6 | R/W | 0h | Enable pipelining for Input 6 Reset type: SYSRSn |
| 29 | PIPE5 | R/W | 0h | Enable pipelining for Input 5 Reset type: SYSRSn |
| 28 | PIPE4 | R/W | 0h | Enable pipelining for Input 4 Reset type: SYSRSn |
| 27 | PIPE3 | R/W | 0h | Enable pipelining for Input 3 Reset type: SYSRSn |
| 26 | PIPE2 | R/W | 0h | Enable pipelining for Input 2 Reset type: SYSRSn |
| 25 | PIPE1 | R/W | 0h | Enable pipelining for Input 1 Reset type: SYSRSn |
| 24 | PIPE0 | R/W | 0h | Enable pipelining for Input 0 Reset type: SYSRSn |
| 23 | SYNC7 | R/W | 0h | Synchronizer Select Control for Input 7 Reset type: SYSRSn |
| 22 | SYNC6 | R/W | 0h | Synchronizer Select Control for Input 6 Reset type: SYSRSn |
| 21 | SYNC5 | R/W | 0h | Synchronizer Select Control for Input 5 Reset type: SYSRSn |
| 20 | SYNC4 | R/W | 0h | Synchronizer Select Control for Input 4 Reset type: SYSRSn |
| 19 | SYNC3 | R/W | 0h | Synchronizer Select Control for Input 3 Reset type: SYSRSn |
| 18 | SYNC2 | R/W | 0h | Synchronizer Select Control for Input 2 Reset type: SYSRSn |
| 17 | SYNC1 | R/W | 0h | Synchronizer Select Control for Input 1 Reset type: SYSRSn |
| 16 | SYNC0 | R/W | 0h | Synchronizer Select Control for Input 0 Reset type: SYSRSn |
| 15-14 | FIN7 | R/W | 0h | Input filter selection for CELL Input 7 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 13-12 | FIN6 | R/W | 0h | Input filter selection for CELL Input 6 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 11-10 | FIN5 | R/W | 0h | Input filter selection for CELL Input 5 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 9-8 | FIN4 | R/W | 0h | Input filter selection for CELL Input 4 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 7-6 | FIN3 | R/W | 0h | Input filter selection for CELL Input 3 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 5-4 | FIN2 | R/W | 0h | Input filter selection for CELL Input 2 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 3-2 | FIN1 | R/W | 0h | Input filter selection for CELL Input 1 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
| 1-0 | FIN0 | R/W | 0h | Input filter selection for CELL Input 0 2 bits are used to define the edge filtering . 00 : No filtering 01 : Rising edge detect 10 : Falling edge detect 11 : Any edge detect Reset type: SYSRSn |
CLB_IN_MUX_SEL_0 is shown in Figure 8-66 and described in Table 8-69.
Return to the Summary Table.
Input selection to decide between Signals and GP register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SEL_GP_IN_7 | SEL_GP_IN_6 | SEL_GP_IN_5 | SEL_GP_IN_4 | SEL_GP_IN_3 | SEL_GP_IN_2 | SEL_GP_IN_1 | SEL_GP_IN_0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R-0 | 0h | Reserved |
| 7 | SEL_GP_IN_7 | R/W | 0h | Select control for Input 7 to decide between external input and CLB_GP_REG[7] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[7] Reset type: SYSRSn |
| 6 | SEL_GP_IN_6 | R/W | 0h | Select control for Input 6 to decide between external input and CLB_GP_REG[6] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[6] Reset type: SYSRSn |
| 5 | SEL_GP_IN_5 | R/W | 0h | Select control for Input 5 to decide between external input and CLB_GP_REG[5] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[5] Reset type: SYSRSn |
| 4 | SEL_GP_IN_4 | R/W | 0h | Select control for Input 4 to decide between external input and CLB_GP_REG[4] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[4] Reset type: SYSRSn |
| 3 | SEL_GP_IN_3 | R/W | 0h | Select control for Input 3 to decide between external input and CLB_GP_REG[3] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[3] Reset type: SYSRSn |
| 2 | SEL_GP_IN_2 | R/W | 0h | Select control for Input 2 to decide between external input and CLB_GP_REG[2] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[2] Reset type: SYSRSn |
| 1 | SEL_GP_IN_1 | R/W | 0h | Select control for Input 1 to decide between external input and CLB_GP_REG[1] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[1] Reset type: SYSRSn |
| 0 | SEL_GP_IN_0 | R/W | 0h | Select control for Input 0 to decide between external input and CLB_GP_REG[0] 0 : Input comes from selected external input 1 : Input comes from CLB_GP_REG[0] Reset type: SYSRSn |
CLB_LCL_MUX_SEL_1 is shown in Figure 8-67 and described in Table 8-70.
Return to the Summary Table.
Input Mux selection for local mux
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| MISC_INPUT_SEL_3 | MISC_INPUT_SEL_2 | MISC_INPUT_SEL_1 | MISC_INPUT_SEL_0 | RESERVED | |||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0-0h | |||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | LCL_MUX_SEL_IN_3 | ||||||
| R-0-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| LCL_MUX_SEL_IN_3 | LCL_MUX_SEL_IN_2 | LCL_MUX_SEL_IN_1 | |||||
| R/W-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| LCL_MUX_SEL_IN_1 | LCL_MUX_SEL_IN_0 | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | MISC_INPUT_SEL_3 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 30 | MISC_INPUT_SEL_2 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 29 | MISC_INPUT_SEL_1 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 28 | MISC_INPUT_SEL_0 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 27-20 | RESERVED | R-0 | 0h | Reserved |
| 19-15 | LCL_MUX_SEL_IN_3 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 3 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 14-10 | LCL_MUX_SEL_IN_2 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 2 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 9-5 | LCL_MUX_SEL_IN_1 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 1 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 4-0 | LCL_MUX_SEL_IN_0 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 0 See Local Signals and Mux Selection Table Reset type: SYSRSn |
CLB_LCL_MUX_SEL_2 is shown in Figure 8-68 and described in Table 8-71.
Return to the Summary Table.
Input Mux selection for local mux
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| MISC_INPUT_SEL_7 | MISC_INPUT_SEL_6 | MISC_INPUT_SEL_5 | MISC_INPUT_SEL_4 | RESERVED | |||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0-0h | |||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | LCL_MUX_SEL_IN_7 | ||||||
| R-0-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| LCL_MUX_SEL_IN_7 | LCL_MUX_SEL_IN_6 | LCL_MUX_SEL_IN_5 | |||||
| R/W-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| LCL_MUX_SEL_IN_5 | LCL_MUX_SEL_IN_4 | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | MISC_INPUT_SEL_7 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 30 | MISC_INPUT_SEL_6 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 29 | MISC_INPUT_SEL_5 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 28 | MISC_INPUT_SEL_4 | R/W | 0h | When this bit is set to 1, the corresponding LCL_MUX_SEL_IN has a range of 32 to 63 Reset type: SYSRSn |
| 27-20 | RESERVED | R-0 | 0h | Reserved |
| 19-15 | LCL_MUX_SEL_IN_7 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 7 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 14-10 | LCL_MUX_SEL_IN_6 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 6 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 9-5 | LCL_MUX_SEL_IN_5 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 5 See Local Signals and Mux Selection Table Reset type: SYSRSn |
| 4-0 | LCL_MUX_SEL_IN_4 | R/W | 0h | 5 bit MUX Select for Local MUX control for Input 4 See Local Signals and Mux Selection Table Reset type: SYSRSn |
CLB_BUF_PTR is shown in Figure 8-69 and described in Table 8-72.
Return to the Summary Table.
PUSH and PULL pointers
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PUSH | RESERVED | PULL | ||||||||||||||||||||||||||||
| R-0-0h | R/W-0h | R-0-0h | R/W-0h | ||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-24 | RESERVED | R-0 | 0h | Reserved |
| 23-16 | PUSH | R/W | 0h | 8 bit pointer which indicates the number of data values which have been pulled from the buffer by the High Level Controller. This counter will wrap around after 0xff. The Least significant 2 bits are used as the actual pointer for the operation. Reset type: SYSRSn |
| 15-8 | RESERVED | R-0 | 0h | Reserved |
| 7-0 | PULL | R/W | 0h | 8 bit pointer which indicates the number of data values that have been written by the High Level controller into the buffer. The Least significant 2 bits are used as the actual pointer for the operation. Reset type: SYSRSn |
CLB_GP_REG is shown in Figure 8-70 and described in Table 8-73.
Return to the Summary Table.
General purpose register for CELL inputs
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| SW_RLS_CTRL_7 | SW_RLS_CTRL_6 | SW_RLS_CTRL_5 | SW_RLS_CTRL_4 | SW_RLS_CTRL_3 | SW_RLS_CTRL_2 | SW_RLS_CTRL_1 | SW_RLS_CTRL_0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| SW_GATING_CTRL_7 | SW_GATING_CTRL_6 | SW_GATING_CTRL_5 | SW_GATING_CTRL_4 | SW_GATING_CTRL_3 | SW_GATING_CTRL_2 | SW_GATING_CTRL_1 | SW_GATING_CTRL_0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| REG | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | SW_RLS_CTRL_7 | R/W | 0h | Software release control for output 7 of the asynchronous output conditioning block Reset type: SYSRSn |
| 30 | SW_RLS_CTRL_6 | R/W | 0h | Software release control for output 6 of the asynchronous output conditioning block Reset type: SYSRSn |
| 29 | SW_RLS_CTRL_5 | R/W | 0h | Software release control for output 5 of the asynchronous output conditioning block Reset type: SYSRSn |
| 28 | SW_RLS_CTRL_4 | R/W | 0h | Software release control for output 4 of the asynchronous output conditioning block Reset type: SYSRSn |
| 27 | SW_RLS_CTRL_3 | R/W | 0h | Software release control for output 3 of the asynchronous output conditioning block Reset type: SYSRSn |
| 26 | SW_RLS_CTRL_2 | R/W | 0h | Software release control for output 2 of the asynchronous output conditioning block Reset type: SYSRSn |
| 25 | SW_RLS_CTRL_1 | R/W | 0h | Software release control for output 1 of the asynchronous output conditioning block Reset type: SYSRSn |
| 24 | SW_RLS_CTRL_0 | R/W | 0h | Software release control for output 0 of the asynchronous output conditioning block Reset type: SYSRSn |
| 23 | SW_GATING_CTRL_7 | R/W | 0h | Software gating control for output 7 of the asynchronous output conditioning block Reset type: SYSRSn |
| 22 | SW_GATING_CTRL_6 | R/W | 0h | Software gating control for output 6 of the asynchronous output conditioning block Reset type: SYSRSn |
| 21 | SW_GATING_CTRL_5 | R/W | 0h | Software gating control for output 5 of the asynchronous output conditioning block Reset type: SYSRSn |
| 20 | SW_GATING_CTRL_4 | R/W | 0h | Software gating control for output 4 of the asynchronous output conditioning block Reset type: SYSRSn |
| 19 | SW_GATING_CTRL_3 | R/W | 0h | Software gating control for output 3 of the asynchronous output conditioning block Reset type: SYSRSn |
| 18 | SW_GATING_CTRL_2 | R/W | 0h | Software gating control for output 2 of the asynchronous output conditioning block Reset type: SYSRSn |
| 17 | SW_GATING_CTRL_1 | R/W | 0h | Software gating control for output 1 of the asynchronous output conditioning block Reset type: SYSRSn |
| 16 | SW_GATING_CTRL_0 | R/W | 0h | Software gating control for output 0 of the asynchronous output conditioning block Reset type: SYSRSn |
| 15-8 | RESERVED | R-0 | 0h | Reserved |
| 7-0 | REG | R/W | 0h | 8 bits which are directly connected to the 8 inputs of the CELL if that corresponding bit is selected in the CLB_IN_MUX_SEL_0 register Reset type: SYSRSn |
CLB_OUT_EN is shown in Figure 8-71 and described in Table 8-74.
Return to the Summary Table.
CELL output enable register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| OUT0 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | OUT0 | R/W | 0h | 32 bits which are directly driven out as OUTPUT_EN signals. Enabling bit x (x = 0:31) will override the corresponding peripheral signal muxed on the CLB OUTx. Reset type: SYSRSn |
CLB_GLBL_MUX_SEL_1 is shown in Figure 8-72 and described in Table 8-75.
Return to the Summary Table.
Global Mux select for CELL inputs
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | GLBL_MUX_SEL_IN_3 | GLBL_MUX_SEL_IN_2 | |||||||||||||
| R-0-0h | R/W-0h | R/W-0h | |||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GLBL_MUX_SEL_IN_2 | GLBL_MUX_SEL_IN_1 | GLBL_MUX_SEL_IN_0 | |||||||||||||
| R/W-0h | R/W-0h | R/W-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RESERVED | R-0 | 0h | Reserved |
| 27-21 | GLBL_MUX_SEL_IN_3 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 3 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 20-14 | GLBL_MUX_SEL_IN_2 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 2 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 13-7 | GLBL_MUX_SEL_IN_1 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 1 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 6-0 | GLBL_MUX_SEL_IN_0 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 0 See Global Signals and Mux Selection Table Reset type: SYSRSn |
CLB_GLBL_MUX_SEL_2 is shown in Figure 8-73 and described in Table 8-76.
Return to the Summary Table.
Global Mux select for CELL inputs
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | GLBL_MUX_SEL_IN_7 | GLBL_MUX_SEL_IN_6 | |||||||||||||
| R-0-0h | R/W-0h | R/W-0h | |||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GLBL_MUX_SEL_IN_6 | GLBL_MUX_SEL_IN_5 | GLBL_MUX_SEL_IN_4 | |||||||||||||
| R/W-0h | R/W-0h | R/W-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RESERVED | R-0 | 0h | Reserved |
| 27-21 | GLBL_MUX_SEL_IN_7 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 7 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 20-14 | GLBL_MUX_SEL_IN_6 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 6 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 13-7 | GLBL_MUX_SEL_IN_5 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 5 See Global Signals and Mux Selection Table Reset type: SYSRSn |
| 6-0 | GLBL_MUX_SEL_IN_4 | R/W | 0h | 7 bit MUX Select for Global MUX control for Input 4 See Global Signals and Mux Selection Table Reset type: SYSRSn |
CLB_PRESCALE_CTRL is shown in Figure 8-74 and described in Table 8-77.
Return to the Summary Table.
Prescaler register control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| PRESCALE | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| PRESCALE | |||||||
| R/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TAP | STRB | CLKEN | ||||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | PRESCALE | R/W | 0h | 16-bit Value of prescaler to be used for the counter as reference to reset when reaching this value. The counter is a simple incrementing counter which will count up to the reference value and reset to 0 and this cycle will continue as long as the counter is enabled. This 16-bit register value is used as a reference for the 16-bit counter to reset to zero whenever count reaches this value. Reset type: SYSRSn |
| 15-6 | RESERVED | R-0 | 0h | Reserved |
| 5-2 | TAP | R/W | 0h | TAP Select value. These 4 bits will be used as a select to tap one of the 16 register bit position of the counter as the output. 0000 selects Counter Bit position 0 0001 selects Counter Bit position 1 .... 1111 selects Counter Bit position 15 Reset type: SYSRSn |
| 1 | STRB | R/W | 0h | When set to 0, a strobe output will be sent out whenever the counter value matches the PRESCALE_VALUE. When set to 1, the output of the counter register bit position as selected by TAP_SELECT_VALUE will be sent out. Reset type: SYSRSn |
| 0 | CLKEN | R/W | 0h | Enable the prescale clock/strobe generator. A 16-bit counter is used to either generate a strobe or send out a selected counter bit position to the CLB CELL. This is meant to be a general purpose strobe/prescaled clock which can be used by the CELL logic if needed. This will be sent to the CELL through one of the LCL_IN MUX ports. Reset type: SYSRSn |
CLB_INTR_TAG_REG is shown in Figure 8-75 and described in Table 8-78.
Return to the Summary Table.
Interrupt Tag register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TAG | ||||||
| R-0-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-6 | RESERVED | R-0 | 0h | Reserved |
| 5-0 | TAG | R/W | 0h | 6 bits which are used by the High Level Controller to set a tag value on flagging interrupts. This can be cleared through the VBUS interface since it is writeable through the VBUS. Reset type: SYSRSn |
CLB_LOCK is shown in Figure 8-76 and described in Table 8-79.
Return to the Summary Table.
Lock control register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| KEY | |||||||
| WSonce-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| KEY | |||||||
| WSonce-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LOCK | ||||||
| R-0-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | KEY | WSonce | 0h | These 16 bits act as a key to enable writes to Bit 0 of this register. The only time a '1' can be written to Bit 0 is by a single 32-bit write where bits 31:16 equal 0x5a5a and bit 0 is '1'. All other writes are ignored including separate 16-bit writes. This is EALLOW protected. Reset type: SYSRSn |
| 15-1 | RESERVED | R-0 | 0h | Reserved |
| 0 | LOCK | R/W | 0h | This bit is used as a one-time write bit (Set Once). Once it is set to '1', only a reset (SYSRSN 0) will clear this bit back to 0. Reset type: SYSRSn |
CLB_HLC_INSTR_READ_PTR is shown in Figure 8-77 and described in Table 8-80.
Return to the Summary Table.
HLC instruction read pointer
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | READ_PTR | ||||||
| R-0-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-5 | RESERVED | R-0 | 0h | Reserved |
| 4-0 | READ_PTR | R/W | 0h | This is a 5 bit value which will be used as an address pointer to read out HLC instruction memory. Reset type: SYSRSn |
CLB_HLC_INSTR_VALUE is shown in Figure 8-78 and described in Table 8-81.
Return to the Summary Table.
HLC instruction read value
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | INSTR | ||||||
| R-0-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| INSTR | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-12 | RESERVED | R-0 | 0h | Reserved |
| 11-0 | INSTR | R | 0h | This is a 12 bit value which will read the content of the HLC instruction memory address pointed by CLB_HLC_INSTR_READ_PTR register. Reset type: SYSRSn |
CLB_DBG_OUT_2 is shown in Figure 8-79 and described in Table 8-82.
Return to the Summary Table.
Visibility for CLB inputs and final asynchronous outputs
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | IN | OUT | |||||||||||||||||||||||||||||
| R/W1C-0h | R/W-0h | R/W-0h | |||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R/W1C | 0h | Reserved |
| 15-8 | IN | R/W | 0h | These bits reflect the state of the 8 inputs finally going to the CELL after selection and input conditioning. Reset type: SYSRSn |
| 7-0 | OUT | R/W | 0h | These bits reflect the state of the 8 outputs of the Output Conditioning Block. Reset type: SYSRSn |
CLB_DBG_R0 is shown in Figure 8-80 and described in Table 8-83.
Return to the Summary Table.
R0 of High level Controller
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_R0 Reset type: SYSRSn |
CLB_DBG_R1 is shown in Figure 8-81 and described in Table 8-84.
Return to the Summary Table.
R1 of High level Controller
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_R1 Reset type: SYSRSn |
CLB_DBG_R2 is shown in Figure 8-82 and described in Table 8-85.
Return to the Summary Table.
R2 of High level Controller
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_R2 Reset type: SYSRSn |
CLB_DBG_R3 is shown in Figure 8-83 and described in Table 8-86.
Return to the Summary Table.
R3 of High level Controller
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_R3 Reset type: SYSRSn |
CLB_DBG_C0 is shown in Figure 8-84 and described in Table 8-87.
Return to the Summary Table.
Count of Unit 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_C0 Reset type: SYSRSn |
CLB_DBG_C1 is shown in Figure 8-85 and described in Table 8-88.
Return to the Summary Table.
Count of Unit 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_C1 Reset type: SYSRSn |
CLB_DBG_C2 is shown in Figure 8-86 and described in Table 8-89.
Return to the Summary Table.
Count of Unit 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| DBG | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | DBG | R | 0h | CLB_DBG_C2 Reset type: SYSRSn |
CLB_DBG_OUT is shown in Figure 8-87 and described in Table 8-90.
Return to the Summary Table.
Outputs of various units in the Cell
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| OUT7 | OUT6 | OUT5 | OUT4 | OUT3 | OUT2 | OUT1 | OUT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| LUT42_OUT | FSM2_LUTOUT | FSM2_S1 | FSM2_S0 | COUNT2_MATCH1 | COUNT2_ZERO | COUNT2_MATCH2 | RESERVED |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-1-1h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| LUT41_OUT | FSM1_LUTOUT | FSM1_S1 | FSM1_S0 | COUNT1_MATCH1 | COUNT1_ZERO | COUNT1_MATCH2 | RESERVED |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-1-1h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| LUT40_OUT | FSM0_LUTOUT | FSM0_S1 | FSM0_S0 | COUNT0_MATCH1 | COUNT0_ZERO | COUNT0_MATCH2 | RESERVED |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | OUT7 | R | 0h | CELL Output 7 Reset type: SYSRSn |
| 30 | OUT6 | R | 0h | CELL Output 6 Reset type: SYSRSn |
| 29 | OUT5 | R | 0h | CELL Output 5 Reset type: SYSRSn |
| 28 | OUT4 | R | 0h | CELL Output 4 Reset type: SYSRSn |
| 27 | OUT3 | R | 0h | CELL Output 3 Reset type: SYSRSn |
| 26 | OUT2 | R | 0h | CELL Output 2 Reset type: SYSRSn |
| 25 | OUT1 | R | 0h | CELL Output 1 Reset type: SYSRSn |
| 24 | OUT0 | R | 0h | CELL Output 0 Reset type: SYSRSn |
| 23 | LUT42_OUT | R | 0h | LUT4_OUT UNIT 2 Reset type: SYSRSn |
| 22 | FSM2_LUTOUT | R | 0h | FSM_LUT_OUT UNIT 2 Reset type: SYSRSn |
| 21 | FSM2_S1 | R | 0h | FSM_S1 UNIT 2 Reset type: SYSRSn |
| 20 | FSM2_S0 | R | 0h | FSM_S0 UNIT 2 Reset type: SYSRSn |
| 19 | COUNT2_MATCH1 | R | 0h | COUNT_MATCH1 UNIT 2 Reset type: SYSRSn |
| 18 | COUNT2_ZERO | R | 0h | COUNT_ZERO UNIT 2 Reset type: SYSRSn |
| 17 | COUNT2_MATCH2 | R | 0h | COUNT_MATCH2 UNIT 2 Reset type: SYSRSn |
| 16 | RESERVED | R-1 | 1h | Reserved |
| 15 | LUT41_OUT | R | 0h | LUT4_OUT UNIT 1 Reset type: SYSRSn |
| 14 | FSM1_LUTOUT | R | 0h | FSM_LUT_OUT UNIT 1 Reset type: SYSRSn |
| 13 | FSM1_S1 | R | 0h | FSM_S1 UNIT 1 Reset type: SYSRSn |
| 12 | FSM1_S0 | R | 0h | FSM_S0 UNIT 1 Reset type: SYSRSn |
| 11 | COUNT1_MATCH1 | R | 0h | COUNT_MATCH1 UNIT 1 Reset type: SYSRSn |
| 10 | COUNT1_ZERO | R | 0h | COUNT_ZERO UNIT 1 Reset type: SYSRSn |
| 9 | COUNT1_MATCH2 | R | 0h | COUNT_MATCH2 UNIT 1 Reset type: SYSRSn |
| 8 | RESERVED | R-1 | 1h | Reserved |
| 7 | LUT40_OUT | R | 0h | LUT4_OUT UNIT 0 Reset type: SYSRSn |
| 6 | FSM0_LUTOUT | R | 0h | FSM_LUT_OUT UNIT 0 Reset type: SYSRSn |
| 5 | FSM0_S1 | R | 0h | FSM_S1 UNIT 0 Reset type: SYSRSn |
| 4 | FSM0_S0 | R | 0h | FSM_S0 UNIT 0 Reset type: SYSRSn |
| 3 | COUNT0_MATCH1 | R | 0h | COUNT_MATCH1 UNIT 0 Reset type: SYSRSn |
| 2 | COUNT0_ZERO | R | 0h | COUNT_ZERO UNIT 0 Reset type: SYSRSn |
| 1 | COUNT0_MATCH2 | R | 0h | COUNT_MATCH2 UNIT 0 Reset type: SYSRSn |
| 0 | RESERVED | R-0 | 0h | Reserved |