SPRACX3 October   2021 F28377D-SEP , F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Trademarks
  2. 1 Introduction
  3. 2 Getting Started With C2000 SysConfig
    1. 2.1 Example C2000 SysConfig in CCS
    2. 2.2 Other SysConfig Tools
  4. 3 C2000 SysConfig Overview
    1. 3.1 Modules
    2. 3.2 PinMux
    3. 3.3 Peripheral Initialization
    4. 3.4 Code Generation
    5. 3.5 Error Detection
    6. 3.6 SysConfig Script File
  5. 4 SysConfig Generated Files After the Project is Built
  6. 5 Application Code Based on C2000 SysConfig Initialization
  7. 6 Interrupt Support
  8. 7 Device-Specific Code Generation
  9. 8 Adding C2000 SysConfig Support to Existing Projects
  10. 9 Remove C2000 SysConfig Support from Projects
  11. 10Standalone SysConfig Tool
  12. 11Summary
  13. 12References

Application Code Based on C2000 SysConfig Initialization

The first step in using the C2000 SysConfig initialization in an application is calling the Board_init or any of the other Module_init functions in the application code. The most common use-case is calling the Board_init after the Device_init function call to initialize all modules configured inside the C2000 SysConfig tool.

After the device initialization calls are completed, any further driverlib function call for using each module should be done using the new application specific name of the module.

Figure 5-1 Application Code Using C2000 SysConfig Initialization

In the example above, the selected instance of the I2C peripheral is I2CA. You can switch to another instance of I2C by changing the GUI to select I2CB, and everything else is automatically taken care of if the application code uses the name assigned to the peripheral in the $name configurable option.