SPNU636 January   2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP

 

  1.   Hercules Software Diagnostic Library CSP Without LDRA
    1.     Trademarks
    2. 1  Introduction
    3. 2  Software Requirements
    4. 3  Software Diagnostic Library TAU Tool Restrictions
    5. 4  Terminologies Used in Software Diagnostic Library TAU
      1. 4.1 What is Unit Testing?
      2. 4.2 What is a Test Sequence?
      3. 4.3 What is a TCF?
      4. 4.4 What is Code Coverage?
      5. 4.5 What is Regression Report?
    6. 5  Functional Blocks of Software Diagnostic Library TAU
    7. 6  Software Diagnostic Library TAU Test Flow
    8. 7  Manual Settings to the LDRA Install Needed by the User
    9. 8  Steps for Using the Software Diagnostic Library TAU
    10. 9  Inputs to Software Diagnostic Library TAU
      1. 9.1 Device Selection
      2. 9.2 Target Configuration File
      3. 9.3 Build Options File
    11. 10 How to Add Individual Test Cases
    12. 11 Reports
      1. 11.1 Regression Report
      2. 11.2 Dynamic Coverage Analysis Report
    13. 12 FAQ

Steps for Using the Software Diagnostic Library TAU

Step 1: Open the Software Diagnostic Library TAU tool.

SafeTI_lib_open_pg_SPNU615.pngFigure 10. Software Diagnostic Library GUI Open Page

Step 2: Select a particular device from the Device Family drop-down menu.

device_fam_select_SPNU615.pngFigure 11. Device Family Selection

Step 3: Browse for the target configuration file and the build options file.

For more information about the target configuration file, see Section 9.2. For more information about the build options file, see Section 9.3.

target_build_option_select_SPNU615.pngFigure 12. Target and Build Option Selection

Step 4: Select the tests to be run, then connect the board and click the “Run” button.

test_case_select_run_SPNU615.pngFigure 13. Test Case Selection and Run

When the build is successful and the .out file is created, the tool starts executing the test cases. The details of the test case execution is shown in a new pop-up window (see Figure 14).

Step 6: Test Execution

test_execution_SPNU615.pngFigure 14. Test Execution

The generated reports are saved in the <install_dir>\Test\<device>\SafetyLibrary\Reports\ folder.

NOTE

Do not close the Software Diagnostic Library TAU window until the test execution is completed or successfully terminated after clicking the Stop button. Never kill the process while the test sequence is under analysis.