SPNU636 January 2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP
The build options file is a text file in the following format:
| Compiler Options: |
| Linker Options: |
| Run time Library: |
| CG Tool Root Path: |
| COMPortNumber: 5 |
| COMPortBaudRate: 9600 |
| COMPortParity: N |
| COMPortDatabits: 8 |
| COMPortStopBits: 2 |
NOTE
The options corresponding to the COMPort are default settings in the corresponding HALCoGen project (default SCI settings) of the device variant. If these settings are changed in the build options file, the test cases will not execute successfully unless the HALCoGen project configuration is also changed and the code is re-generated.
Some sample build options files are provided in the folder <install directory>\Test\Misc\BuildOptions.
Users can use it as is in their project.
NOTE
These settings must be in sync with the HALCoGen project corresponding to the device as in the demo_app\HALCoGen.
Step 1: Compiler Option Selection
Figure 15. Compiler Option Select Step 2: Linker Option Selection
Figure 16. Linker Option Select Step 3: Runtime Library Selection
Figure 17. Runtime Library Selection