SPNU636 January   2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS2135-S , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP

 

  1.   Hercules Software Diagnostic Library CSP Without LDRA
    1.     Trademarks
    2. Introduction
    3. Software Requirements
    4. Software Diagnostic Library TAU Tool Restrictions
    5. Terminologies Used in Software Diagnostic Library TAU
      1. 4.1 What is Unit Testing?
      2. 4.2 What is a Test Sequence?
      3. 4.3 What is a TCF?
      4. 4.4 What is Code Coverage?
      5. 4.5 What is Regression Report?
    6. Functional Blocks of Software Diagnostic Library TAU
    7. Software Diagnostic Library TAU Test Flow
    8. Manual Settings to the LDRA Install Needed by the User
    9. Steps for Using the Software Diagnostic Library TAU
    10. Inputs to Software Diagnostic Library TAU
      1. 9.1 Device Selection
      2. 9.2 Target Configuration File
      3. 9.3 Build Options File
    11. 10 How to Add Individual Test Cases
    12. 11 Reports
      1. 11.1 Regression Report
      2. 11.2 Dynamic Coverage Analysis Report
    13. 12 FAQ

How to Add Individual Test Cases

Add a new folder and type “MyTests” in the test folder created by the tool. Define the test sequence and save it in the folder “Test1” inside MyTests. Figure 18 shows a template of a test sequence. Add more test sequences by adding more folders in MyTests.

test_seq_template_SPNU615.pngFigure 18. Test Sequence Template

Folder structure as shown in Figure 19 must be followed strictly.

SDL_CSP_TestFileFolderStructure.pngFigure 19. Folder Structure

NOTE

  • The Excel sheets must be saved as .xlsx and not .xls.
  • One test folder must contain only one test sequence.
  • The sheet containing the test cases must be named “Test”. Other sheets in the workbook are ignored.

Points to keep in mind while writing a test sequence:

  • The test sequence must begin with “TCF Description” and end with “End of Test Sequence”.
  • The global declarations and code must be inserted in the beginning of the test sequence after TCF description.
  • User Declarations, Startup code, and Cleanup code (if needed) must be inserted above each test case.
  • The test case description, ID, and requirements covered for each test case must be inserted above each test case.
  • The total number of parameters of the test case (including the function input parameters, return value, and global variables checked) must be mentioned for each test case, as shown in Figure 20 and Figure 21.
  • The file under test must be mentioned for each test case, and the function tested must be defined in each file.
  • Two test cases must be separated by a blank row.
  • End of the test sequence must be written in column 3 after the last test case. Leave a blank row after each test case.
  • Each test sequence can test only one file.
  • The Excel sheet must be saved as *_UT.xlsx (where UT stands for Unit Test). A code coverage report is also generated along with the regression report.

Figure 20 and Figure 21 show a few examples of a test case.

test_case_example_SPNU615.pngFigure 20. Test Case Example 1
test_case_example_2_SPNU615.pngFigure 21. Test Case Example 2

Tip: Right-click on the test list field and click “Refresh” to regenerate the list.