SPNU151V January 1998 – February 2020
You can get feedback about your code from the ULP (Ultra-Low Power) Advisor. For a list and descriptions of the ULP rules, see www.ti.com/ulpadvisor. You can enable/disable the rules using any of the following. Using multiple --advice options on the command line is permitted.
The --advice:power option enables checking specified ULP Advisor rules. The syntax is:
| --advice:power={all|none|rulespec} |
The rulespec parameter is a comma-separated list of rule numbers to enable. For example, --advice:power=1.1,7.2,7.3,7.4 enables rules 1.1, 7.2, 7.3, and 7.4.
The --advice:power_severity option sets the diagnostic severity for ULP Advisor rules. The syntax is:
| --advice:power_severity={error|warning|remark|suppress} |
The syntax of the pragmas is:
| #pragma CHECK_ULP ("{all|none|rulespec}") |
| #pragma RESET_ULP ("{all|rulespec}") |