SPNU151V January 1998 – February 2020
;***********************************************************
;* FUNCTION VENEER: $max *
;***********************************************************
$max:
.state16
BX pc
NOP
.state32
B _max
.text
.global _max
;***********************************************************
;* FUNCTION DEF: _max *
;***********************************************************
_max:
CMP A1, A2
MOVLE A1, A2
BX LR
Since sum( ) is a 16-bit function, its entry point is $sum. Because it was compiled for dual-state interworking, an alternate entry point, _sum, located in a different section is included. All calls to sum( ) requiring a state change use the _sum entry point.
The call to max( ) in sum( ) references $max, because sum( ) is a 16-bit function. If max( ) were a 16-bit function, sum( ) would call the actual entry point for max( ). However, since max( ) is a 32-bit function, $max is the alternate entry point for max( ) and handles the state change required by sum( ).