SPNU151V January 1998 – February 2020
Addresses of functions taken in 16-BIS state use the address of the 16-BIS state entry point to the function (with bit 0 of the address set). Likewise, addresses of functions taken in 32-BIS state use the address of the 32-BIS state entry point (with bit 0 of the address cleared). Then all indirect calls are performed by loading the address of the called function into a register and executing the branch and exchange (BX) instruction. This automatically changes the state and ensures that the code works correctly, regardless of what state the address was in when it was taken.
The return address must also be set up so that the state of the processor is consistent and known upon return. Bit 0 of the address is tested to determine if the BX instruction invokes a state change. If it does not invoke a state change, the return address is set up for the state of the function. If it does invoke a change, the return address is set up for the alternate state and code is executed to return to the function's state.
Because the entry point into a function depends upon the state of the function that takes the address, it is more efficient to take the address of a function when in the same state as that function. This ensures that the address of the actual function is used, not its alternate entry point. Because the indirect call can invoke a state change itself, entering a function through its alternate entry point, even if calling it from a different state, is unnecessary.
Example 11 shows sum( ) calling max( ) with code that is compiled for the 16-BIS state and supports dual-state interworking. The sum( ) function is compiled with the -code_state=16 option, which creates 16-bit instructions for pre-UAL assembly code. (Refer to the ARM Assembly Language Tools User's Guide for information on UAL syntax.) Example 14 shows the same function call with code that is compiled for the 32-BIS state and supports dual-state interworking. Function max( ) is compiled without the -code_state=16 option, creating 32-bit instructions.