SPNU151V January 1998 – February 2020
Built-in functions are predefined by the compiler. They can be called like a regular function, but they do not require a prototype or definition. The compiler supplies the proper prototype and definition.
The ARM compiler supports the following built-in functions:
void *_ _curpc(void);
int _ _run_address_check(void);