SPNU151V January 1998 – February 2020
By default, the compiler allows dual-state interworking between functions. However, the compiler allows you to alter the level of support to meet your particular needs.
In dual-state interworking, it is the called function's responsibility to handle the proper state changes required by the calling function. It is the calling function's responsibility to handle the proper state changes required to indirectly call a function (call it by address). Therefore, a function supports dual-state interworking if it provides the capability for functions requiring a state change to directly call the function (call it by name) and provides the mechanism to indirectly call functions involving state changes.
If a function does not support dual-state interworking, it cannot be called by functions requiring a state change and cannot indirectly call functions that support dual-state interworking. Regardless of whether a function supports dual-state interworking or not, it can directly or indirectly call certain functions:
Given this definition of dual-state support, the ARM C/C++ compiler offers three levels of support. Use Table 6-8 to determine the best level of support to use for your code.
If your code... | Use this level of support ... |
---|---|
Requires few state changes | Default |
Requires many state changes | Optimized |
Requires no state changes and has frequent indirect calls | None |
Here is detailed information about each level of support:
Functions with this support level can indirectly call only functions that do not require a state change and do not support dual-state interworking. Because functions with this support level do not provide dual-state interworking, they cannot be called by a function requiring a state change.
Use this support level if you do not require dual-state interworking, have frequent indirect calls, and cannot tolerate the additional code size or speed incurred by the indirect calls supporting dual-state interworking.
When a program does not require any state changes, the only difference between specifying no support and default support is that indirect calls are more complex in the default support level.