SPNU151V January 1998 – February 2020
When you link your program, you must specify the object library as one of the linker input files so that references to the I/O and run-time-support functions can be resolved. You can either specify the library or allow the compiler to select one for you. See Section 4.3.1 for further information.
When a library is linked, the linker includes only those library members required to resolve undefined references. For more information about linking, see theARM Assembly Language Tools User's Guide.
C, C++, and mixed C and C++ programs can use the same run-time-support library. Run-time-support functions and variables that can be called and referenced from both C and C++ will have the same linkage.
If you want to link object files created with the TI CodeGen tools with object files generated by other compiler tool chains, the ARM standard specifies that you should define the _AEABI_PORTABILITY_LEVEL preprocessor symbol as follows before #including any standard header files, such as <stdlib.h>.
#define _AEABI_PORTABILITY_LEVEL 1
This definition enables full portability. Defining the symbol to 0 specifies that the "C standard" portability level will be used.