SPNU151V January 1998 – February 2020
Application Binary Interface (ABI) defines the low level interface between object files, and between an executable and its execution environment. An ABI allows ABI-compliant object files to be linked together, regardless of their source, and allows the resulting executable to run on any system that supports that ABI.
Object files conforming to different ABIs cannot be linked together. The linker detects this situation and generates an error.
The ARM compiler now supports only the Embedded Application Binary Interface (EABI) ABI, which uses the ELF object format and the DWARF debug format. If you want support for the legacy TI_ARM9_ABI and TIARM ABIs, please use the ARM v5.2 Code Generation Tools and refer to SPNU151J and SPNU118J for documentation.
An industry consortium founded by ARM Ltd defined a standard ABI for binary code intended for the ARM architecture. This ABI is called the Application Binary Interface (ABI) for the ARM Architecture Version 2 (ARM ABIv2). This ABI is also referred to as Embedded Application Binary Interface (EABI). The terms ABIv2 and EABI can be used interchangeably.
For more details on the ABI, see Section 5.13.