SPNU151V January 1998 – February 2020
#pragma SET_CODE_SECTION("func1")
extern void func1();
#pragma SET_CODE_SECTION()
...
void func1() { ... }
In Example 8 func1 is placed in section func1. If conflicting sections are specified at the declaration and definition, a diagnostic is issued.
The current CODE_SECTION and DATA_SECTION pragmas and GCC attributes can be used to override the SET_CODE_SECTION and SET_DATA_SECTION pragmas. For example: